rexnord.com | Home Page Information
rexnord.com | Power Transmission
 
rexnord.com | Industry Menu

NORTH AMERICA

1-866-REXNORD (U.S.)

1-414-643-2366 (INT)

 

rexnord.com > Power Transmission > Industries > Cement

Storage Dome & Reclamation System with Unique Gear Drive

Let Lafarge Corp. Use Fly Ash for Cement Mixture

Cement Industry ALPENA, Mich. - The installation of a new, state-of-the-art storage and handling facility has allowed the Lafarge Corporation to use fly ash in its raw cement materials mixture. The use of fly ash will let the Alpena, Michigan, plant, the largest cement production facility in North America, produce a cement with wider applications, having lower alkali properties and offer its customers both Type I and II cement. The plant currently produces 2.3 million tons of cement per year. To improve its cement quality, reduce the amount of raw materials used in the cement manufacturing process, and eliminate shale-related environmental concerns, the Lafarge Corporation's cement plant decided to change its raw materials cement mixture. Lafarge substituted silica sand and fly ash for shale. The mixture change meant several things for Lafarge. First, the substitution would allow them to reduce the large amount of virgin natural resources, such as shale, it was using in producing cement. Used in the cement mixture instead of shale would be fly ash, a recyclable waste product of coal-fired power generation plants, and silica sand found in taconite left over from the iron ore extraction process. Secondly, Lafarge could eliminate the environmental concerns they had with disposing a large percentage of the high-sulfur cement kiln dust (CKD) that resulted from shale processing.


"It was mainly an environmental concern," noted Lafarge Engineering Manager Steve Cayton. "During processing, a high concentration of sulfur separates out in the shale burning process. So what we would do is throw away - actually waste - some of the valuable kiln dust because of the high level of sulfur it contained. With fly ash and silica sand, we no longer have the high level of sulfur in the kiln dust. Also, the shale hydrocarbon emissions that were generated during production were considered volatile. Those substances will no longer be present." Previously, these hydrocarbons had to be extracted through a costly and time consuming process.


Solving the Problem of Fly Ash Storage

Lafarge's plan to change mixtures seemed like a good switch except for one problem - the physical properties of fly ash made it costly and impractical because it is difficult to handle and store. Fly ash is a light powdery material that can literally blow away in an open-air environment. Lafarge wanted to keep the fly ash totally enclosed in order to prevent any of the material from becoming airborne. They believed that an enclosed system would provide the best solution from an environmental protection standpoint. A state-of-the art handling system had to be designed to implement the use of fly ash.


After an examination of several storage methods, Lafarge decided on a 40,000-ton capacity concrete storage unit with an automated reclamation system from the Salt Lake City, Utah-based company, Cambelt International.


Cambelt International works closely with Dome Technology of Idaho Falls, Idaho, in the design and construction of automated reclamation systems. Dome Technology builds the storage domes and Cambelt supplies overall project management and designs the unique reclamation system for the storage domes.


"Lafarge's situation was unique," said Cambelt's Vice President of Marketing Rexnord Wood. "They needed to handle and reclaim a very difficult to handle material that was previously impractical to use."


Designing the Reclaim Drive System

While Cambelt's automated dome reclamation technology was proven in several applications, Lafarge's requirements offered several "custom" challenges for the automated dome reclamation system designers.


For example, a special drive system was needed to meet the extremely high overhung load produced by the system's chain drive. Cambelt had been employing a European manufactured gear drive in previous dome applications. However, Lafarge requested that Falk gear drives be used on their dome system.


"We're glad they did," said Cambelt's Wood. "They were ready to come to Salt Lake City to discuss our needs and their creative solution proved invaluable." Initially, Cambelt was working with the local sales office. Because Cambelt required a "custom" solution, the local office called in engineers from the headquarters in Milwaukee.


Rexnord account executive Ted Shushereba noted that they were able to provide Cambelt a unique, application-engineered system from standard products.


"Cambelt needed an enlarged, high-strength, low-speed shaft and bearings because of the very high overhung load on the system's chain drive. Cambelt gave us some design criteria that tested the limits of our standard product offering," said Shushereba. "We had to analyze each stressed component of the unit to determine its suitability for the application."


To better understand Cambelt's needs, engineers went to Salt Lake City to meet and discuss alternative drive system solutions. Rather than design an expensive, custom gear drive from scratch, engineers were able to provide a "custom" solution utilizing two standard gear drives, a shaft-mount and a foot-mount, working in tandem. This enabled the company to deliver the drives in the time-frame Lafarge required and at a lower cost.


"Additionally, we were able to adapt a low-speed shaft from our standard mixer gear drive line to accommodate the high overhung load," said Shushereba. The tandem drive has a primary drive mounted to the vertical parallel shaft gear drive's high-speed shaft to achieve the low, 0.5 rpm on the low-speed shaft that Cambelt required for the rotating center column on the reclaim system.


The drive assembly to rotate the center column consists of a chain and sprocket driven by the Falk modified tandem gear drive. It's powered by a 7.5 HP (5.6 kW) AC electric motor with an output of 1750 rpm. The tandem drive gives the system a 3,386:1 gear reduction ratio with a total of six reductions. Total output torque of the drive system is 860,000 lb-in. (97,172 Nm). The entire drive system is located atop the dome in a drive house.


Also key to the drive system's success was the Falk solid steel plate housing. "Some other gear housings are cast iron - which are very stiff - but are weak at the non-uniform curvatures of the cast," said Shushereba. "Cast housings have been known to break on applications with very high overhung load," he added.


Because of its patented Magnum No-Leak shaft seals, Shushereba notes that the Falk drives are suited to working in the extremely dusty environment found in the fly ash storage dome drive house. "A purgeable grease chamber and contact seal prevent the infiltration of dirt and grime into the drive bearings. A unique drain-back passage works in conjunction with a radial and axial bushing seal to effectively retain oil and eliminate leaks," said Shushereba.


"This is important," said Lafarge's Cayton. "Any oil leaks from the drive could possibly contaminate the fly ash."


The Falk drives also have an efficient splash lubrication system to ensure that Lafarge's column rotation drive system stays lubricated. A motor-driven pump with a filter and flow switch provide constant, positive lubrication to the drives' helical gearing.


"What we have found with European drives is that in many cases the repair parts are more difficult to get and the delivery time is longer," said Cayton. In cases of some gear drives, of which Lafarge has 500-plus at the Alpena facility, Cayton said that many of the European drives had to be sent back to Germany for repairs. "This leads to downtime that is very costly for our operation. We lose an estimated $24,000 every hour any part of our production system is down. If we have a choice with gear drives, we'd rather use Falk...," noted Cayton.


The Dome Reclamation System

Cambelt's mechanical reclaim system allows the inside of the storage dome to be fully utilized, sacrificing only a small part of the dome's volume for the reclamation system. The system pulls the material, in this case fly ash, to the center of the floor through a controlled discharge opening into an air-slide conveyor in a tunnel under the dome floor.


A bridge truss (additional trusses are optional) is attached to the base of a center column equipped with screw conveyor and powered by an electric motor. Tag screws and trailing shrouds can also be installed depending on the nature and flow ability of the stored materials.


The system's center column is mounted on a thrust bearing and a radial bearing, and connected to a fabricated support base. At the top of the center column, a hoist is mounted to raise and lower the truss to the level of the fly ash. Retrieval of the stored fly ash is by means of a 30-inch (76.2 cm) diameter, 90-foot (27.4 m) long radial screw that turns while the center of the column drive rotates the screw truss through 360 degrees of the dome.


The dome is filled from the top with a pneumatic conveyor feeding in the fly ash. A pneumatic conveyor is required to handle the light, powdery fly ash.


The system gathers the fly ash to the opening in the center of the dome floor to the air-slide conveyor that outloads it to the raw grind area where it is combined with silica sand and eventually sent to kilns for the removal of any water or carbon dioxide. This process produces a mixture commonly called "clinker." The clinker is either stored, or combined with gypsum and processed in roller presses and ball mills for the final finish grinding. The discharge from the ball mill is transported to high-efficiency separators where it is separated into the finished cement product.


Changing the System Provides Benefits for Lafarge

Cambelt's reclamation system allows for 100 percent of stored materials to be reclaimed from Lafarge's 40,000-ton storage dome. For Lafarge, the reclamation system has had a greater impact than just being able to handle and reclaim a difficult material. By being able to use fly ash and silica sand instead of shale, Lafarge is changing its Type I portland cement to a newer low alkali product that will allow for a greater range of uses in its markets. Cayton adds that because the consistency of the quality of the raw materials has improved with fly ash, customers will be able to get a greater consistency in the cement they purchase. Customers will be able to store a Lafarge cement that meets both Type I and Type II specifications. This translates into a less expensive, yet higher quality product for the customer.


 

 

Please answer a few quick questions to help us make this site better!
 
Mission Statement | Corporate Profile | Legal Information | Terms and Conditions of Sale
 
© Copyright 1995 - Rexnord Industries, LLC.
All rights reserved.