rexnord.com | Home Page Information
CAREERS   
rexnord.com | Power Transmission
 

NORTH AMERICA

1-866-REXNORD (U.S.)

1-414-643-2366 (INT)

 

rexnord.com > Power Transmission > Customer Support > Technical_Information > New High-Efficiency Gearmotors Offer Energy Savings Over Worm Gear Drives

New High-Efficiency Gearmotors Offer Energy Savings Over Worm Gear Drives

In 1992, Congress passed the Energy Policy and Conservation Act that imposes new efficiency requirements on manufacturers of electric motors, lamps, utility distribution transformers and luminaires. This also means that motor manufacturers will be required to produce general purpose single-speed motors that are more efficient, and use less energy than previous makes. This act, which demands compliance by October 1997, is also having a dramatic effect on power transmission manufacturers and their current gearmotor designs. Add to this new legislation, large incentives offered by power companies to customers using these new efficient motors, and it's easy to see that the future of power transmission products will be driven by the customer's need for more efficient, environmentally friendly products.


In this new climate of conservation and manufacturer's responsibility, the Falk Ultramite® has been developed as a new, high-efficiency gearmotor for a wide range of general purpose, factory, and low-horsepower power transmission applications.


The premise behind the Ultramite gearmotor is energy savings over the traditional worm gear drive. Unlike a worm gear drive, this gearmotor is designed to be lower in initial cost. Because the gear teeth are so efficient, the customer can specify a smaller horsepower, less expensive motor. The result is a product that is initially less expensive and saves a considerable amount of energy over long term service life.


Smaller, Lower Cost Motors

Because the Ultramite's gear teeth are more efficient than those on worm gear drives, motor selections can be one size smaller. One size smaller motors can be used in over one-third of possible single reduction worm gear selections and the majority of double reduction worm-worm gear selections. This reduces the cost of the motor for the Ultramite system and may also increase motor efficiency if the smaller motor is operating closer to its full rating.


Substitutions, drop-in replacement and retrofits are made easy due to the Ultramite gearmotor's base-mounted design that has a footprint that matches those of other major manufacturers. A simple, plug-in and bolt-on design makes this new drive compatible with standard, off-the-shelf NEMA and IEC C-face motors permitting the use of customer-preferred brands. The Ultramite is available in several sizes in the .25 HP (.25 kW) to 20 HP (15 kW) power range. (See figure 1., Smaller Motors and figure 2., Motor Savings)




This isn't to say that worm gear drives are obsolete...they aren't. Worm gear drives are still well-suited to certain applications and are fairly cost-efficient and have acceptable reliability. Worm gear drives perform best in limited duty applications. For example, a good application for a worm gear drive would be raising and lowering a parking gate or an industrial garage door. However, worm gear drives are a poor choice where efficiency is required.


Long Term Energy Cost Savings

The Ultramite has an operating efficiency that is considerably higher than a worm gear drive. The beveled, helical-toothed gearing is hardened to enhance design efficiency and extend service life. The combination of the helical gearing and smaller electric motor give the Ultramite a substantial operating cost savings. (See figure 3., Efficiency Comparison)



Motor Efficiency

The aforementioned energy conservation laws are already affecting the way industry buys. Even though the regulating agencies are not currently penalizing companies for purchasing less efficient equipment, many companies are specifying the more efficient equipment. (See figure 4., Average Motor Efficiency)



The energy cost savings the Ultramite provides is calculable. This can be figured two ways: Long Method The annual energy cost savings of an Ultramite drive over a worm gear drive can be calculated using this relatively complex formula:


Where:
S = Annual Energy Cost Saving T = Operating Time (hrs/yr)
L = Demand Load (Output HP) em = Electric Motor Efficiency
.746 = kW Per Horsepower ew = Worm Gear Drive Efficiency
R = Electrical Energy Rate eu = Ultramite Drive Efficiency
Short Method

This calculation can be simplified using appropriate charts to find values for factors:


S = (L) x (C) x (D)


Where:


S = Annual Energy Cost Savings ($)


L = Demand Load (Output HP) - (Refer to figure 5., Estimated Demand Load)


C = (.746)(R)(T)/em, (Refer to figure 6., Factor C)


D = [ 1/ew - 1/ew ] (Refer to Figure 7., Factor D)


Electrical Energy Rate

The electrical energy rate ($/kW hr) for a particular industrial user, is equal to the monthly electric utility bill, divided by the number of kilowatt hours used during the month. Rates vary throughout the country and are based on several different charges and rate structures. Consult the local power utility for information.


Example - Energy Cost Savings


Calculate the energy cost savings to replace a worm gear drive with an Ultramite drive using the short method:


Worm Drive Ultramite
Demand Load 1.3 HP 1.3 HP
Duty Cycle 6,000 Hrs/Yr 6,000 Hrs/Yr
Energy Rate $.08/kWHr $.08/kWHr
Drive Size 4.25" C.D. 07UCB2
Drive Ratio 60:1 63:1
Drive Efficiency 65% 97%
Motor Size 2 HP 1 HP
Motor Efficiency 86.5% 87.5%
System Efficiency 56.2% 84.9%

ENERGY COST SAVINGS Year Annual Cumulative
S = (L) x (C) x (D) 1 $273 $273
S = (1.3) x ($414.20) x (.5075) 2 $273 $564
S = $273.20 3 $273 $820
4 $273 $1093
5 $273 $1366

Please answer a few quick questions to help us make this site better!
 
Mission Statement | Corporate Profile | Legal Information | Terms and Conditions of Sale
 
© Copyright 1995 - Rexnord Industries, LLC.
All rights reserved.