rexnord.com | Home Page Information
CAREERS   
rexnord.com | Power Transmission
 
rexnord.com | Industry Menu

NORTH AMERICA

1-866-REXNORD (U.S.)

1-414-643-2366 (INT)

 

rexnord.com > Power Transmission > Industries > Electric Generating Dam

The San Roque Project

Setting a Goal

The San Roque Project is a $700 million multi-purpose embankment dam project, located in the town of San Roque, in the province of Pangasinan, on the island of Luzon, in the Philippines. The entire project consists of a dam, power plant, concrete chute spillway to allow excess water to bypass the dam, diversion tunnels to re-route the river past the dam site during onstruction, and an electrical substation.

Once completed, the dam will be 3,600 feet (1,097 meters) long and 650 feet (198 meters) high, making it the largest dam in Asia, and the 12th largest embankment dam in the world. Along with providing an additional power source to the people of Luzon, the dam will harness the water of the Agno River, and help irrigate more than 215,000 acres (87,000 hectares) of agricultural land. Further, it will reduce, by at least 50 percent, the amount of perennial flooding that takes place each year, inundating communities and destroying millions of pesos worth of crops vital to the economy of the region.

The dam also has the potential to have a huge impact on the local tourist economy. Japanese investors have been watching the area, with the intent of building new hotels and water sports facilities for skiing, rowing and fishing.

But, before the dam could be constructed, the San Roque Power Commission had to move millions of tons of earth from one location to another to dig tunnels and connect the two mountains that lay across a deep gorge.


Background

In March 1998, Raytheon Engineers & Constructors was awarded the contract to build the San Roque dam. Faris Engineers & Associates of Bellvue, Washington was the consulting engineering firm working for Raytheon to develop the initial design and specification of the conveying system and auxiliary components.

"By bringing all of the contractors under common control, Raytheon became the project's turn key contractor," said Michael O'Connor of Falk. "The company became responsible for the overall financing and execution of the entire project."

Raytheon had planned to accomplish the task of constructing the dam by asking their standard list of multi-industry OEMs to bid on the design and supply the respective systems necessary to complete the project. However, as the company began to collect proposals from the OEMs, they realized that the project would come in significantly over budget.

Rather than start the project in the red, and only working with specific OEMs, the decision was made to change course and to rely more heavily on internal resources.

Under the new plan, Raytheon would take responsibility for specifying and purchasing the gear drives, pulleys, idlers, belts and structural steel components necessary to construct the conveyor system that would move the earth during construction of the dam.

The original design specified by Faris consisted of a parallel shaft, foot-mounted gear drive. The Wisconsin-Chicago sales office had initial contact with Roberts & Schaffer out of Chicago during the budgetary quotation stages. Roberts & Schaffer was one of the original OEMs initially quoting the conveyor system to Raytheon.

Since first being offered, the RFQ had undergone several revisions. The final version calling for a complete drive package with motors, backstops and brakes. The mechanical spreadsheet, engineered and developed by Faris, specified non competitive gear drives.

"When the prints were generated with the respective part numbers & gear drive sizes they all had Dodge-Flender drive sizes," said O'Connor. "For some reason, there was a tremendously competitive slant away from our company. According to Raytheon, there was no good answer as to why we weren't invited to participate."

In addition to the slanted specifications, O'Connor noted that the timeline called for shipment by the end of September, with delivery to the construction site by the end of 1999.

"That meant the company awarded the contract, would have a previously unheard of deadline of 22 weeks manufacture and ship approximately 40, 500hp and 800hp gear drives."

Thanks to our positive image in the industry, the company was invited to submit a bid for gears drives to be used on the San Roque project.


Product Recommendation

The proposal submitted suggested use of the company's Alignment Free Drive™ - a right-angle, shaft-mounted gear drive featuring bolt-together construction.

"When we first developed the Alignment Free Drive and compared it with the installed cost for a conventional bedplate mounted drive, we realized that the Alignment Free Drive could result in start-up savings of up to 20 percent," said O'Connor. "Since Raytheon was extremely budget conscious about this project, we knew that the cost savings potential would have a positive impact on their decision."

O'Connor said that the Alignment Free Drive would also appeal to Raytheon because it would allow the company to standardize on only two gear drive sizes. In addition, the drives' simple registered fits and bolt-together construction would help to overcome the low skill and language barriers of workers in the field.

"It comes as a completely assembled package," said O'Connor. "All they have to do is connect the head shaft pulley to a hollow quill, torque it down, fasten it, connect the torque arm, and it's ready to go."


Showing Up Unannounced

The initial proposal was conceived and developed approximately 48 hours after receipt of the RFQ – an extremely fast turnaround time for a project of this size.

While unable to schedule an appointment with Raytheon engineering personnel to present the proposal, our engineers and sales representatives chose to travel three hours to Raytheon headquarters, show up unannounced, and attempt to hand deliver the document.

The cold call strategy worked. Upon initial review, Raytheon found the proposal to be attractive, but with one final hurdle. Raytheon had specified a 1.5 service factor. Our conservative approach to developing service factor numbers brought the company's service factor ratings in between 1.29 and 1.36 – too low for approval.

But, after careful scrutiny by both Raytheon and the company's outside engineering consultant, our drives were deemed "technically acceptable" with a 1.25 service factor over motor horsepower and a 1.5 service factor over brake horsepower.

Only two weeks after being informed of the opportunity to bid on the project, we received a letter of intent, accepting the company's proposal for manufacture and shipment of 36 Alignment-Free gear drives, low speed backstops, steelflex and fluid couplings, and motors.

"Two weeks from being informed to acceptance of proposal - talk about making your head spin," said O'Connor.

The Falk Alignment Free Drive™ is currently being used in an overland conveyor system at the future site of the San Roque dam. The system is transporting earth and rock to a process plant where they will be used in the construction of the San Roque Dam in the Philippines. The projected should be completed by the year 2003.


 

 

Please answer a few quick questions to help us make this site better!
 
Mission Statement | Corporate Profile | Legal Information | Terms and Conditions of Sale
 
© Copyright 1995 - Rexnord Industries, LLC.
All rights reserved.