rexnord.com | Home Page Information
CAREERS   
rexnord.com | Power Transmission
 
rexnord.com | Industry Menu

NORTH AMERICA

1-866-REXNORD (U.S.)

1-414-643-2366 (INT)

 

rexnord.com > Power Transmission > Industries > Pet Food

New Shaft-Mounted Gear Drives Speed Production at "Fast Feed" Company

Hudson Protein's unique shaft-mounted speed reducer utilizes a single-taper, torque assist, bushing for fast installation and removal in adverse conditions. NOEL, MO -- Hudson Protein is in the fast feed business. The pet food ingredient company produces more than 1.0 million pounds of feed a week from poultry by-products in a process that demands speed and reliability from employees and equipment alike. As such, when equipment goes down, it must be replaced immediately.
 
The company explored several ways of increasing horsepower and gradually starting the conveyor to reduce the damaging effects of belt slippage and over-torqued motors. They looked at soft-start options including fluid couplings, soft start starters and wound rotor motors. Eventually, Drummond settled on a system incorporating fluid couplings and dual conveyor drives. "Soft start is very important if you want to keep your belt together and you want your motors to last," notes Chetopa's Chief Electrician Bill Kosmus.
 
Recently, bearing failures on a key shaft-mounted speed reducer led Hudson Protein to explore a unique alternative to "typical" shaft-mounted drives as a replacement. A Falk Quadrive® shaft mounted speed reducer, designed around a single-taper "Torque Assist" TA Taper® bushing, met Hudson Protein's challenge for fast installation and removal.
 
"The bearings kept going bad on the old speed reducer," says Hudson Protein Maintenance Supervisor Russell Waymack. "If we lose a gear box on a cooker, we get behind real quick. If we can't cook, we can't run."
 
The ailing shaft-mounted drive was a key component on one of Hudson's seven batch cookers. The 5'x 14' cookers handle 6,000 to 9,000 pounds of feathers or meat for about two hours at temperatures up to 270?F degrees. It is then pressed into feed and cooled before shipment to blending mills and pet food manufacturers around the country.
 
Installation of the drive is dramatically different from past designs. With the bushing in place on the shaft, the speed reducer's tapered bore is moved into place over the bushing and a threaded nut and set screw tightened. The bushing design evenly draws the speed reducer onto the shaft.
 
Previously, Hudson Protein used shaft-mounted speed reducers with a twin-taper bushing design. During installation, inboard and outboard bushings must be aligned with the shaft and unit keyways. Bushing fasteners are alternately tightened (like lugs on an automobile wheel) into threaded holes in the reducer's backup plate; then torqued to specifications. If unevenly torqued, binding and wobbling can occur.
 
Maintenance Leadman Bob Ballard appreciates the simple installation of the single-taper design. "Installation was a lot easier with the torque assist bushing than with the twin-taper design," he says. "There aren't as many parts and the single, threaded-taper was easy to use."

Importance of Uptime

Fast installation shortens downtime, which is important in an operation that runs 24 hours a day up to six days a week. Because, in addition to keeping production output high, Hudson Protein crews also need to be concerned with incoming poultry. Hudson's food division, located in an adjacent building, continually ships raw poultry products 16 hours a day, five days a week.
 
Says Waymack: "We've got raw material coming in from next door all day long," Waymack adds. "Just because we lose a speed reducer doesn't mean the shipments are going to stop. We've got to process it as soon as it comes in or it will spoil. It is extremely important that this reducer run."
 
With these concerns in mind, Neil Snyder, a representative of power transmission distributor Motion Industries, recommended the Falk Quadrive shaft-mounted drive with Torque Assist taper bushing. The Quadrive, with 25:1 ratio, was matched with a 50 hp, 1750 rpm motor producing 35 rpm output on the low speed side of the drive system.
 
Service factor received a boost from about 1.5 to 2.5. Service factor is a formula that combines external load dynamics, reliability, and gear life of a speed reducer and is used to calculate equivalent horsepower capacity. Each application has its own conditions and operating requirements.
 
"We wanted a drive that gave a lot of service and was easily serviceable," notes Waymack. "It had to be able to hold up to the heat and torque."
 
Compact housings and non-complicated gearing also attracted Waymack to the speed reducer since worn equipment, including speed reducers, is often rebuilt to save money. "Simplicity is what we are looking for," he says. "Time is money. If we can rebuild a reducer quickly, that saves us money."

Harsh Environment

High service factor and easy serviceability ensure a long life for the drive, which operates in one of Hudson Protein's harshest applications. Located in the lower level, cooker equipment runs in extreme heat and exposure to abrasive chemicals. Condensation speeds equipment wear. And, variations in cooker loads test the durability of the drive system.
 
Additionally, adverse conditions make bushings susceptible to corroding and fretting to shafts in the high heat and humidity.
 
The design of the single-taper drive assures minimal removal time. The bushing nut is locked in position; the v-belt drive is removed; the high-speed shaft is rotated to develop torque which is multiplied by the gear ratio; and the created mechanical advantage frees the unit from the bushing taper.
 
Ballard finds the design offers significant time savings during removal compared to twin-taper and straight bore designs.
 
"We've fought with twin-taper shaft-mounted drives a long time to get them off the shaft," Ballard adds. "Removal isn't a problem with the torque assist bushing design."
 
Twin-taper bushings present several challenges during removal. In many cases, the threaded removal holes in the flange can become badly corroded and strip out, requiring the bushing to be broken with a sledge hammer. Additionally, opposed twin tapers must be moved along the shaft out of the unit taper, a maneuver which often proves difficult.

Extending Equipment Life

Combating the damaging conditions is no easy task. Current maintenance programs call for routine oil checks of speed reducers. Lubrication plays an especially important role.
 
"The reducer has to have the right lubricant to keep it cool," he says.
 
Stack fans alleviate some of the overheating concerns and oil filters keep lubricant clean longer, despite difficult conditions.
 
Most importantly, by using a unique speed reducer with better reliability and service characteristics, Waymack has improved his production potential as well as reduced the overall maintenance costs. Over time, other cookers will receive the new speed reducers.
 
"There is not a whole lot of maintenance needed to keep this speed reducer running," Waymack adds. "We expect to get many good years of operation out of this speed reducer."

 

 

Please answer a few quick questions to help us make this site better!
 
Mission Statement | Corporate Profile | Legal Information | Terms and Conditions of Sale
 
© Copyright 1995 - Rexnord Industries, LLC.
All rights reserved.