rexnord.com | Home Page Information
rexnord.com | Power Transmission
 
rexnord.com | Aggregate Industsry Menu

NORTH AMERICA

1-866-REXNORD (U.S.)

1-414-643-2366 (INT)

 

rexnord.com > Power Transmission > Industries > Cement And Aggregate > Aggregate

New Shaft-Mounted Drive Technology
Solves Old Installation/Removal Headaches

BIRMINGHAM, AL -- A new shaft-mount speed reducer design gave Vulcan Materials-Dolcito a time-saving option recently when a twin-tapered shaft-mounted drive needed to be replaced on a conveyor feeding one of the company's crushers. A shaft-mounted speed reducer was installed in half the time due to a unique single-tapered bushing design.


"With the tapered bushing, all we had to do was slide the bushing onto the shaft," says Maintenance Manager Jerry Champion.


With the bushing in place on the shaft, the speed reducer's tapered bore was moved into place over the bushing and a threaded nut and set screw tightened. The bushing design provides a uniform draw of the speed reducer onto the shaft.


The torque assist TA Taper® bushing is a feature of the Quadrive®, the newest Falk shaft-mounted speed reducer. A 7.5 hp motor powers Vulcan Material's Quadrive. The low speed shaft turns at 70 rpm processing a maximum capacity of 220 tons per hour (tph) while operating at 330 feet per minute on Vulcan's conveyor with 18-foot pulley shaft centers.


"The Quadrive, with the torque assist taper bushing, is easy to put on since there is only one key to line up and fewer parts than a twin-taper design," notes Champion.


"With twin-taper shaft-mounted drives, you have two bushings and the gear box to line up in one keyway," he adds. "And, there are six to eight bolts to tighten and line up. This can be very difficult, especially if you're in a tight spot on an above-ground platform and pressed for room."


Problems With Straight-Bore Design

Straight bore designs offer no simple solutions, either, since the shaft has to be in near perfect condition. Says Champion: "Straight bore drives are difficult to install as well because you have to be sure that the shaft is clean. And even then, straight-bore speed reducers, often times, don't go on the shaft easily."


Vulcan Materials-Dolcito is a subsidiary of Vulcan Materials Corp., a 36-year-old company with 122 plants across the United States and Mexico and 1991 sales of $1.7 billion.


Up to 30 conveyors (two of which have pulley shaft centers of 272 feet) move material throughout Vulcan Material-Dolcito. More than 1.5 million tons of limestone, sand and gravel, and other lightweight material are processed yearly.


Installing and maintaining quality equipment helps Vulcan Materials meet its annual production goals. That is why at first sign a leakage problem was developing, the old shaft-mounted drive was replaced with the Quadrive.


And, while installation of the unit saved some time, removal of the shaft-mounted drive with the new bushing is expected to take far less time compared to other drive designs. The TA Taper bushing design marks an end to the need for hammering and the damaging results.


Simplified Removal

The threaded nut set screw is loosened and an optional removal tool is attached to lock the bushing nut (standard tools can also be used). When the high-speed shaft is turned, the drive's mechanical advantage powers the unit free from the bushing taper.


This will come as welcome relief to Champion who confronted a host of problems during removal of the twin-taper shaft mounted drive. While the drive was located in an easily accessible location (10 feet off the ground), the conveyor hindered Champion's ability to free the unit from the shaft through pounding, a common method of drive removal.


"It took us well over an hour to pound off the old unit from the shaft. It would have taken us much longer if we were higher up," Champion remembers. "The biggest problem with the twin-taper design is that you have to wedge the drive off. If you can get the bushings to move, you've got it. But, a lot of times the bushings are frozen to the shaft."


In some cases, he adds, a portable power source is required to push the shaft-mounted drives free. "It's a lot more time consuming, especially if you are up in the air," Champion notes.


Additionally, the result of pounding or forcing the drive from the shaft often leads to damaged or ruined equipment, which doesn't exactly meet the Vulcan Material philosophy of maintaining equipment.


"The bushings are often ruined. Sometimes the oil seals are cracked. And, in extreme situations, the speed reducer is damaged beyond repair," Champion notes.


The Quadrive shaft-mounted drive solved other problems for Vulcan Materials as well.


"With the Falk unit, we didn't have to worry about shaft length," adds Champion."The bushing mounts on the back of the drive, so we had some shaft to play with. With the twin-taper design, you have to make sure you have enough shaft for both bushings."


Welcome Change

Plant Manager Welton Hawkins, a 29-year veteran of the aggregate industry, is impressed with this latest bushing technology. "I'm amazed at the developments to shaft-mounted speed reducers within the past 10 years," Hawkins says. "In the past, every shaft-mounted drive was straight bore. There were no tapered-bushing designs available for removing a unit economically and without damage. Now, the time involved in installation and removal has been greatly reduced."


Champion agrees. "Straight bore shaft-mounted drives make you struggle to get the drive all the way off the shaft. With the tapered bushing design, once you get the drive loose from the bushing taper, it'll pop right off," he says.


As a result of the simplified installation and removal, Hawkins plans to specify the single-tapered bushing type shaft- mounted speed reducers on any drives that need to be replaced in the future.


"My first selection criteria is the single-taper type," he notes. "I also look for the easiest shaft-mounted drives to install and remove. And, of course, the drive needs to be the right size for the application."


Prolonging Equipment Life

In addition, Hawkins studies the service factors of all the equipment in the plant. In fact, to safeguard against unplanned downtime, Hawkins frequently orders equipment with capacity up to 20 percent more than required. "If I'm running at close to 220 tph, I know that my equipment can go faster if needed," Hawkins notes.


He combines this cushion with a rigorous continuous predictive maintenance program to combat equipment failures. Speed reducer oil is changed twice a year and oil samples are tested for any premature bearing wear. Monthly grease purges are also conducted.


"You could have the best speed reducer in the world and the bearings could drag it to death due to poor lubrication habits," Hawkins says.


Hawkins also follows strict rules for loading the equipment. "The feed controller has a lot to do with the life of a speed reducer. Not properly regulating the workload, or splurging, can ruin a drive," he says.


To date, after six months of operation, the Quadrive single- taper shaft mounted drive with TA Taper bushings has performed above expectations. "We haven't had any problems with leaking or wobbles," says Champion. "The seals are designed well since they aren't exposed to the elements. This should prolong the life of the drive."


In fact, the Quadrive design features an "inboard" bushing design complemented with severe-duty grease purged seals to protect the high-speed bearings.


Simplified installation and removal play a critical role in the life of a shaft-mounted speed reducer. Forcing the drive on or off the shaft can cause undue stresses to the equipment, not to mention wasted time and energy. This latest technological development in the design of shaft-mounted speed reducers will give Vulcan Materials maintenance crews a time-saving advantage during future changeouts.


 

 

Please answer a few quick questions to help us make this site better!
 
Mission Statement | Corporate Profile | Legal Information | Terms and Conditions of Sale
 
© Copyright 1995 - Rexnord Industries, LLC.
All rights reserved.