rexnord.com | Home Page Information
CAREERS   
rexnord.com | Power Transmission
 
rexnord.com | Industry Menu

NORTH AMERICA

1-866-REXNORD (U.S.)

1-414-643-2366 (INT)

 

rexnord.com > Power Transmission > Industries > Bulk Handling Facility

Bulk Handling Facility

The following is the comparison of the couplings we use now and the new Wrapflex Coupling we should change to. This will show that it is not only cheaper than the one we now have but it is more user friendly. The range of savings just for the part is from 39% to 50% not to mention the time element involved (man hours) is cut from one or two hours depending if you have to move the motor mounts to 5 min.

 

By comparison it shouldn't be hard to see the need to change our system to make us more effective in the eyes of mail flow control. With this new coupling we can turn a break down that was taking 2 hours to a zone call and get the equipment back in service in record time compared to the past.

 

The Area people are spending a lot of money and time to make the company a more effective and cost effective unit. I think it is time we look into ways we can assist in that effort. I feel this new coupling will start us in the right direction and what a feather in our cap if it were to go nationally.

 

This coupling comes with a slide chart, to make it easier for us to match the right coupling to the right application and also has a 3-year warranty.

 

 

Please answer a few quick questions to help us make this site better!
 
Mission Statement | Corporate Profile | Legal Information | Terms and Conditions of Sale
 
© Copyright 1995 - Rexnord Industries, LLC.
All rights reserved.