rexnord.com | Home Page Information
CAREERS   
rexnord.com | Power Transmission
 
rexnord.com | Industry Menu

NORTH AMERICA

1-866-REXNORD (U.S.)

1-414-643-2366 (INT)

 

rexnord.com > Power Transmission > Industries > Mining > Coal Mine

Drummond Controls Conveyor Start to Boost Production Demands

Drummond Controls Conveyor Start to Boost Production Demands When Drummond Coal added a second continuous miner on each of the two sections at its Chetopa mine, essentially doubling the mine's output potential, production forecasts heralded an initial increase of as much as 1,000 tons per day. But, lack of horsepower on Drummond's slope belt conveyor drive system threatened to stop these goals short of daily projected output of 3,700 tons.
 
The company explored several ways of increasing horsepower and gradually starting the conveyor to reduce the damaging effects of belt slippage and over-torqued motors. They looked at soft-start options including fluid couplings, soft start starters and wound rotor motors. Eventually, Drummond settled on a system incorporating fluid couplings and dual conveyor drives. "Soft start is very important if you want to keep your belt together and you want your motors to last," notes Chetopa's Chief Electrician Bill Kosmus.


Problem

Drummond's original drive system, built around a single drive and 300 hp wound rotor motor, powered the existing slope belt with headpulley discharge and snub pulley. While the wound rotor motor provided a moderate level of soft startup, its erratic, jerking motion during start up created problems with other drive system components. For instance, the wound rotor motor caused the loaded conveyor belt to slip during startup as resistance, built up in the motor, was released through the system in stages. The power surges defeated the belt tension created by the snub pulley, causing damaging slippage.


"The belt was slipping every day," says Kosmus. "The slippage got to the point that sometimes you could see the belt smoking." The conveyor belt was not the only component to suffer during startup. The wound rotor motor and drive worked overtime to build up enough torque to start moving the loaded conveyors.


"There were times when we would have to go down in the mine and take coal off the belt just to get it started," says Kosmus.


Despite these efforts, motors were frequently damaged during startup. "The wound rotor motor caused a lot of overloading since the motor sees all of the load from the beginning," he says. "We botched a number of motors just during start up and stopping."


As one of Drummond Coal's medium sized mines, Chetopa depends on its 144 employees (120 miners) to bring high-grade clean coal from the Mary Lee seam. The downtime began to haunt Drummond crews."We could change out a motor in four or five hours, but that's four or five hours of lost production. Now, half a day of downtime could cost us up to 2,000 tons of coal," says Kosmus.


Solution

To solve the slippage problems and boost conveyor speed, Sam Gilbert, Mine Superintendent, and Kosmus first contacted Continental Conveyor & Equipment (Winfield, AL). Together with Continental Conveyor they installed a dual pulley drive system with remote discharge and fluid couplings for a true soft start.


The system incorporates two Falk double-reduction, parallel shaft gear drives connected to 250 hp induction motors. The gear drives feature a 17.10:1 ratio, which produces 68.4 output rpm from an input of 1,170 rpm.


An extended delay fill chamber with adjustable metering allows initial torque transferred by the coupling to be as low as 40 percent of the full load requirement of the conveyor. In a typical startup, the motor comes up to full speed while the coupling gradually engages the pulley. Startup time can be adjusted to more than a minute.


"The fluid couplings are nice since you can bring up your motors to full speed before the belt starts to work," Kosmus adds.


The design also permits excellent motor starting control. Both motors are started at the same time and the fluid couplings allow both to come up to speed in the same time. "The motors' amperage is within 2 or 3 amps of each other during startup," notes Kosmus.


As insurance against conveyor jams, a trip switch on the fluid couplings shuts down the electrical system when fluid coupling oil reaches a predetermined temperature. Without the safety measure, motors can burn out when a conveyor stalls.


To further enhance drive system life, Continental Conveyor boosted the thermal capacity of the drives with shaft-mounted fans. The fans reduce the damaging effects of overheating like lubrication breakdown and premature bearing wear. They also allowed the use of smaller, less expensive gear drives.


"We used to have a floor fan blowing on the gear drive. It would still get hot enough to fry eggs," says Kosmus.


Perhaps most importantly, however, the configuration allowed Drummond to increase belt speed to 650 fpm while eliminating belt slippage.


"The wound rotor motor gave us soft start through resistance. It caused a lot of motor overloading," says Kosmus. "There is no comparison between fluid couplings and wound rotor motors. Startup with fluid couplings is smooth whether or not you've got a load on the belt."


As another soft start option, Kosmus and Gilbert considered the soft start starters. While the electronic starter offered better control than wound rotor motors, its cost was up to three times as expensive as fluid couplings. Past experiences also influenced their decision. "I had used soft start starters in the past," remembers Kosmus. "They either wouldn't come up to speed fast enough or they would come up too hard." Surprisingly, installation of the fluid coupling/dual drive system resulted in no interruption in production.


Drummond-Chetopa relied on Continental Conveyor to build the base plate and belt pulleys. Otherwise, the mine counted on its own ingenuity to complete the remainder of the installation project including the design and construction of a control box.


"We set ourselves up during the week for the installation of the system. The pulleys went in on one Saturday and the following Saturday we tied everything else in," says Kosmus. "We lost no production time."


 

 

Please answer a few quick questions to help us make this site better!
 
Mission Statement | Corporate Profile | Legal Information | Terms and Conditions of Sale
 
© Copyright 1995 - Rexnord Industries, LLC.
All rights reserved.